This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867CS: DP83867CS

Part Number: DP83867CS

I see this question has been asked many different ways but looking for best recommendation for connecting two PHYs (DP83867's) board to board across a backplane (just a few inches)?  I could go transformerless, 1 transformer or 2 transformers since board space is not an issue.

Which is best for 1000BASE (1GbE) operation.

1) transformerless (capacitive coupled)

2) 1 transformer (single transformer between the PHYs center tap with decoupling cap on each side)

3) 2 transformers (2 transformers back to back with center tap decoupling cap on phy side, 50ohm termination in between)

Thanks.