This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8042A: I2C supply

Part Number: TUSB8042A

Dear team,

Is the I2C communication able to operate at 1.8V?

From datasheet: The external interface is enabled when both the SCL/SMBCLK and SDA/SMBDAT pins are pulled up to 3.3 V at the de-assertion of reset.

From this I would assume that it should be 3.3V. Can you confirm?

Thank you for your help.

Kind regards,

Aida