This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS250DF410: DS100DF410 retimer register configuration values for 10G single Lane XFI interface

Part Number: DS250DF410
Other Parts Discussed in Thread: DS100DF410

Hi Team,

We are designing a 10G link between two separate boards. Board 1 has Marvell's cavium processor CN8350 SOC and Board2 has TI-6638K2k SOC. The 10G link is implemented over xfi interface. It uses single differential pair for 10.3125 speed. Both the board are connected together using midplane via edge finger connector.

A retimer IC  DS100DF410 is connected at the Rx line of each board. We tried to figure out the configuration sequence of the retimer. Which I am attaching in this mail thread. Kindly verify whether this register sequence is correct.

We are able to detect the eth interface at both the SOC. But we are not able to send and receive any data over the lines.  We are doubtful about the correct retimer register sequence.

Kindly suggest other methods, if any,  to debug the link.  please clarify what values we should keep to bring up a XFI interface supporting 10G link speed.

0x0	Shared Registers_0x00	00
0x1	Shared Registers_0x01	70
0x2	Shared Registers_0x02	00
0x3	Shared Registers_0x03	00
0x4	Shared Registers_0x04	01
0x5	Shared Registers_0x05	10
0x6	Shared Registers_0x06	00
0x7	Shared Registers_0x07	05
0xFF	Global Registers_0xFF	04
0x0	Channel 0_0x00	00
0x1	Channel 0_0x01	00
0x2	Channel 0_0x02	00
0x3	Channel 0_0x03	00
0x4	Channel 0_0x04	00
0x5	Channel 0_0x05	00
0x6	Channel 0_0x06	00
0x7	Channel 0_0x07	00
0x8	Channel 0_0x08	00
0x9	Channel 0_0x09	00
0xA	Channel 0_0x0A	10
0xB	Channel 0_0x0B	0F
0xC	Channel 0_0x0C	08
0xD	Channel 0_0x0D	00
0xE	Channel 0_0x0E	93
0xF	Channel 0_0x0F	69
0x10	Channel 0_0x10	3A
0x11	Channel 0_0x11	20
0x12	Channel 0_0x12	E0
0x13	Channel 0_0x13	30
0x14	Channel 0_0x14	00
0x15	Channel 0_0x15	10
0x16	Channel 0_0x16	7A
0x17	Channel 0_0x17	36
0x18	Channel 0_0x18	40
0x19	Channel 0_0x19	23
0x1A	Channel 0_0x1A	00
0x1B	Channel 0_0x1B	03
0x1C	Channel 0_0x1C	24
0x1D	Channel 0_0x1D	00
0x1E	Channel 0_0x1E	E9
0x1F	Channel 0_0x1F	00
0x20	Channel 0_0x20	00
0x21	Channel 0_0x21	00
0x22	Channel 0_0x22	00
0x23	Channel 0_0x23	40
0x24	Channel 0_0x24	00
0x25	Channel 0_0x25	00
0x26	Channel 0_0x26	00
0x27	Channel 0_0x27	00
0x28	Channel 0_0x28	00
0x29	Channel 0_0x29	00
0x2A	Channel 0_0x2A	30
0x2B	Channel 0_0x2B	00
0x2C	Channel 0_0x2C	72
0x2D	Channel 0_0x2D	80
0x2E	Channel 0_0x2E	00
0x2F	Channel 0_0x2F	06
0x30	Channel 0_0x30	00
0x31	Channel 0_0x31	00
0x32	Channel 0_0x32	11
0x33	Channel 0_0x33	88
0x34	Channel 0_0x34	3F
0x35	Channel 0_0x35	1F
0x36	Channel 0_0x36	31
0x37	Channel 0_0x37	00
0x38	Channel 0_0x38	00
0x39	Channel 0_0x39	00
0x3A	Channel 0_0x3A	A5
0x3B	Channel 0_0x3B	00
0x3C	Channel 0_0x3C	00
0x3D	Channel 0_0x3D	00
0x3E	Channel 0_0x3E	80
0x3F	Channel 0_0x3F	00
0x40	Channel 0_0x40	00
0x41	Channel 0_0x41	01
0x42	Channel 0_0x42	04
0x43	Channel 0_0x43	10
0x44	Channel 0_0x44	40
0x45	Channel 0_0x45	08
0x46	Channel 0_0x46	02
0x47	Channel 0_0x47	80
0x48	Channel 0_0x48	03
0x49	Channel 0_0x49	0C
0x4A	Channel 0_0x4A	30
0x4B	Channel 0_0x4B	41
0x4C	Channel 0_0x4C	50
0x4D	Channel 0_0x4D	C0
0x4E	Channel 0_0x4E	60
0x4F	Channel 0_0x4F	90
0x50	Channel 0_0x50	88
0x51	Channel 0_0x51	82
0x52	Channel 0_0x52	A0
0x53	Channel 0_0x53	46
0x54	Channel 0_0x54	52
0x55	Channel 0_0x55	8C
0x56	Channel 0_0x56	B0
0x57	Channel 0_0x57	C8
0x58	Channel 0_0x58	57
0x59	Channel 0_0x59	5D
0x5A	Channel 0_0x5A	69
0x5B	Channel 0_0x5B	75
0x5C	Channel 0_0x5C	D5
0x5D	Channel 0_0x5D	99
0x5E	Channel 0_0x5E	96
0x5F	Channel 0_0x5F	A5
0x60	Channel 0_0x60	00
0x61	Channel 0_0x61	00
0x62	Channel 0_0x62	00
0x63	Channel 0_0x63	00
0x64	Channel 0_0x64	00
0x65	Channel 0_0x65	00
0x66	Channel 0_0x66	00
0x67	Channel 0_0x67	20
0x68	Channel 0_0x68	00
0x69	Channel 0_0x69	0A
0x6A	Channel 0_0x6A	22
0x6B	Channel 0_0x6B	40
0x6C	Channel 0_0x6C	40
0x6D	Channel 0_0x6D	40
0x6E	Channel 0_0x6E	00
0x6F	Channel 0_0x6F	00
0x70	Channel 0_0x70	03
0x71	Channel 0_0x71	00
0x72	Channel 0_0x72	00
0x73	Channel 0_0x73	00
0x74	Channel 0_0x74	00
0x75	Channel 0_0x75	00
0x0	Channel 1_0x00	00
0x1	Channel 1_0x01	00
0x2	Channel 1_0x02	00
0x3	Channel 1_0x03	00
0x4	Channel 1_0x04	00
0x5	Channel 1_0x05	00
0x6	Channel 1_0x06	00
0x7	Channel 1_0x07	00
0x8	Channel 1_0x08	00
0x9	Channel 1_0x09	00
0xA	Channel 1_0x0A	10
0xB	Channel 1_0x0B	0F
0xC	Channel 1_0x0C	08
0xD	Channel 1_0x0D	00
0xE	Channel 1_0x0E	93
0xF	Channel 1_0x0F	69
0x10	Channel 1_0x10	3A
0x11	Channel 1_0x11	20
0x12	Channel 1_0x12	E0
0x13	Channel 1_0x13	30
0x14	Channel 1_0x14	00
0x15	Channel 1_0x15	10
0x16	Channel 1_0x16	7A
0x17	Channel 1_0x17	36
0x18	Channel 1_0x18	40
0x19	Channel 1_0x19	23
0x1A	Channel 1_0x1A	00
0x1B	Channel 1_0x1B	03
0x1C	Channel 1_0x1C	24
0x1D	Channel 1_0x1D	00
0x1E	Channel 1_0x1E	E9
0x1F	Channel 1_0x1F	00
0x20	Channel 1_0x20	00
0x21	Channel 1_0x21	00
0x22	Channel 1_0x22	00
0x23	Channel 1_0x23	40
0x24	Channel 1_0x24	00
0x25	Channel 1_0x25	00
0x26	Channel 1_0x26	00
0x27	Channel 1_0x27	00
0x28	Channel 1_0x28	00
0x29	Channel 1_0x29	00
0x2A	Channel 1_0x2A	30
0x2B	Channel 1_0x2B	00
0x2C	Channel 1_0x2C	72
0x2D	Channel 1_0x2D	80
0x2E	Channel 1_0x2E	00
0x2F	Channel 1_0x2F	06
0x30	Channel 1_0x30	00
0x31	Channel 1_0x31	00
0x32	Channel 1_0x32	11
0x33	Channel 1_0x33	88
0x34	Channel 1_0x34	3F
0x35	Channel 1_0x35	1F
0x36	Channel 1_0x36	31
0x37	Channel 1_0x37	00
0x38	Channel 1_0x38	00
0x39	Channel 1_0x39	00
0x3A	Channel 1_0x3A	A5
0x3B	Channel 1_0x3B	00
0x3C	Channel 1_0x3C	00
0x3D	Channel 1_0x3D	00
0x3E	Channel 1_0x3E	80
0x3F	Channel 1_0x3F	00
0x40	Channel 1_0x40	00
0x41	Channel 1_0x41	01
0x42	Channel 1_0x42	04
0x43	Channel 1_0x43	10
0x44	Channel 1_0x44	40
0x45	Channel 1_0x45	08
0x46	Channel 1_0x46	02
0x47	Channel 1_0x47	80
0x48	Channel 1_0x48	03
0x49	Channel 1_0x49	0C
0x4A	Channel 1_0x4A	30
0x4B	Channel 1_0x4B	41
0x4C	Channel 1_0x4C	50
0x4D	Channel 1_0x4D	C0
0x4E	Channel 1_0x4E	60
0x4F	Channel 1_0x4F	90
0x50	Channel 1_0x50	88
0x51	Channel 1_0x51	82
0x52	Channel 1_0x52	A0
0x53	Channel 1_0x53	46
0x54	Channel 1_0x54	52
0x55	Channel 1_0x55	8C
0x56	Channel 1_0x56	B0
0x57	Channel 1_0x57	C8
0x58	Channel 1_0x58	57
0x59	Channel 1_0x59	5D
0x5A	Channel 1_0x5A	69
0x5B	Channel 1_0x5B	75
0x5C	Channel 1_0x5C	D5
0x5D	Channel 1_0x5D	99
0x5E	Channel 1_0x5E	96
0x5F	Channel 1_0x5F	A5
0x60	Channel 1_0x60	00
0x61	Channel 1_0x61	00
0x62	Channel 1_0x62	00
0x63	Channel 1_0x63	00
0x64	Channel 1_0x64	00
0x65	Channel 1_0x65	00
0x66	Channel 1_0x66	00
0x67	Channel 1_0x67	20
0x68	Channel 1_0x68	00
0x69	Channel 1_0x69	0A
0x6A	Channel 1_0x6A	22
0x6B	Channel 1_0x6B	40
0x6C	Channel 1_0x6C	40
0x6D	Channel 1_0x6D	40
0x6E	Channel 1_0x6E	00
0x6F	Channel 1_0x6F	00
0x70	Channel 1_0x70	03
0x71	Channel 1_0x71	00
0x72	Channel 1_0x72	00
0x73	Channel 1_0x73	00
0x74	Channel 1_0x74	00
0x75	Channel 1_0x75	00
0x0	Channel 2_0x00	00
0x1	Channel 2_0x01	00
0x2	Channel 2_0x02	00
0x3	Channel 2_0x03	00
0x4	Channel 2_0x04	00
0x5	Channel 2_0x05	00
0x6	Channel 2_0x06	00
0x7	Channel 2_0x07	00
0x8	Channel 2_0x08	00
0x9	Channel 2_0x09	00
0xA	Channel 2_0x0A	10
0xB	Channel 2_0x0B	0F
0xC	Channel 2_0x0C	08
0xD	Channel 2_0x0D	00
0xE	Channel 2_0x0E	93
0xF	Channel 2_0x0F	69
0x10	Channel 2_0x10	3A
0x11	Channel 2_0x11	20
0x12	Channel 2_0x12	E0
0x13	Channel 2_0x13	30
0x14	Channel 2_0x14	00
0x15	Channel 2_0x15	10
0x16	Channel 2_0x16	7A
0x17	Channel 2_0x17	36
0x18	Channel 2_0x18	40
0x19	Channel 2_0x19	23
0x1A	Channel 2_0x1A	00
0x1B	Channel 2_0x1B	03
0x1C	Channel 2_0x1C	24
0x1D	Channel 2_0x1D	00
0x1E	Channel 2_0x1E	E9
0x1F	Channel 2_0x1F	00
0x20	Channel 2_0x20	00
0x21	Channel 2_0x21	00
0x22	Channel 2_0x22	00
0x23	Channel 2_0x23	40
0x24	Channel 2_0x24	00
0x25	Channel 2_0x25	00
0x26	Channel 2_0x26	00
0x27	Channel 2_0x27	00
0x28	Channel 2_0x28	00
0x29	Channel 2_0x29	00
0x2A	Channel 2_0x2A	30
0x2B	Channel 2_0x2B	00
0x2C	Channel 2_0x2C	72
0x2D	Channel 2_0x2D	80
0x2E	Channel 2_0x2E	00
0x2F	Channel 2_0x2F	06
0x30	Channel 2_0x30	00
0x31	Channel 2_0x31	00
0x32	Channel 2_0x32	11
0x33	Channel 2_0x33	88
0x34	Channel 2_0x34	3F
0x35	Channel 2_0x35	1F
0x36	Channel 2_0x36	31
0x37	Channel 2_0x37	00
0x38	Channel 2_0x38	00
0x39	Channel 2_0x39	00
0x3A	Channel 2_0x3A	A5
0x3B	Channel 2_0x3B	00
0x3C	Channel 2_0x3C	00
0x3D	Channel 2_0x3D	00
0x3E	Channel 2_0x3E	80
0x3F	Channel 2_0x3F	00
0x40	Channel 2_0x40	00
0x41	Channel 2_0x41	01
0x42	Channel 2_0x42	04
0x43	Channel 2_0x43	10
0x44	Channel 2_0x44	40
0x45	Channel 2_0x45	08
0x46	Channel 2_0x46	02
0x47	Channel 2_0x47	80
0x48	Channel 2_0x48	03
0x49	Channel 2_0x49	0C
0x4A	Channel 2_0x4A	30
0x4B	Channel 2_0x4B	41
0x4C	Channel 2_0x4C	50
0x4D	Channel 2_0x4D	C0
0x4E	Channel 2_0x4E	60
0x4F	Channel 2_0x4F	90
0x50	Channel 2_0x50	88
0x51	Channel 2_0x51	82
0x52	Channel 2_0x52	A0
0x53	Channel 2_0x53	46
0x54	Channel 2_0x54	52
0x55	Channel 2_0x55	8C
0x56	Channel 2_0x56	B0
0x57	Channel 2_0x57	C8
0x58	Channel 2_0x58	57
0x59	Channel 2_0x59	5D
0x5A	Channel 2_0x5A	69
0x5B	Channel 2_0x5B	75
0x5C	Channel 2_0x5C	D5
0x5D	Channel 2_0x5D	99
0x5E	Channel 2_0x5E	96
0x5F	Channel 2_0x5F	A5
0x60	Channel 2_0x60	00
0x61	Channel 2_0x61	00
0x62	Channel 2_0x62	00
0x63	Channel 2_0x63	00
0x64	Channel 2_0x64	00
0x65	Channel 2_0x65	00
0x66	Channel 2_0x66	00
0x67	Channel 2_0x67	20
0x68	Channel 2_0x68	00
0x69	Channel 2_0x69	0A
0x6A	Channel 2_0x6A	22
0x6B	Channel 2_0x6B	40
0x6C	Channel 2_0x6C	40
0x6D	Channel 2_0x6D	40
0x6E	Channel 2_0x6E	00
0x6F	Channel 2_0x6F	00
0x70	Channel 2_0x70	03
0x71	Channel 2_0x71	00
0x72	Channel 2_0x72	00
0x73	Channel 2_0x73	00
0x74	Channel 2_0x74	00
0x75	Channel 2_0x75	00
0x0	Channel 3_0x00	00
0x1	Channel 3_0x01	00
0x2	Channel 3_0x02	00
0x3	Channel 3_0x03	00
0x4	Channel 3_0x04	00
0x5	Channel 3_0x05	00
0x6	Channel 3_0x06	00
0x7	Channel 3_0x07	00
0x8	Channel 3_0x08	00
0x9	Channel 3_0x09	00
0xA	Channel 3_0x0A	10
0xB	Channel 3_0x0B	0F
0xC	Channel 3_0x0C	08
0xD	Channel 3_0x0D	00
0xE	Channel 3_0x0E	93
0xF	Channel 3_0x0F	69
0x10	Channel 3_0x10	3A
0x11	Channel 3_0x11	20
0x12	Channel 3_0x12	E0
0x13	Channel 3_0x13	30
0x14	Channel 3_0x14	00
0x15	Channel 3_0x15	10
0x16	Channel 3_0x16	7A
0x17	Channel 3_0x17	36
0x18	Channel 3_0x18	40
0x19	Channel 3_0x19	23
0x1A	Channel 3_0x1A	00
0x1B	Channel 3_0x1B	03
0x1C	Channel 3_0x1C	24
0x1D	Channel 3_0x1D	00
0x1E	Channel 3_0x1E	E9
0x1F	Channel 3_0x1F	00
0x20	Channel 3_0x20	00
0x21	Channel 3_0x21	00
0x22	Channel 3_0x22	00
0x23	Channel 3_0x23	40
0x24	Channel 3_0x24	00
0x25	Channel 3_0x25	00
0x26	Channel 3_0x26	00
0x27	Channel 3_0x27	00
0x28	Channel 3_0x28	00
0x29	Channel 3_0x29	00
0x2A	Channel 3_0x2A	30
0x2B	Channel 3_0x2B	00
0x2C	Channel 3_0x2C	72
0x2D	Channel 3_0x2D	80
0x2E	Channel 3_0x2E	00
0x2F	Channel 3_0x2F	06
0x30	Channel 3_0x30	00
0x31	Channel 3_0x31	00
0x32	Channel 3_0x32	11
0x33	Channel 3_0x33	88
0x34	Channel 3_0x34	3F
0x35	Channel 3_0x35	1F
0x36	Channel 3_0x36	31
0x37	Channel 3_0x37	00
0x38	Channel 3_0x38	00
0x39	Channel 3_0x39	00
0x3A	Channel 3_0x3A	A5
0x3B	Channel 3_0x3B	00
0x3C	Channel 3_0x3C	00
0x3D	Channel 3_0x3D	00
0x3E	Channel 3_0x3E	80
0x3F	Channel 3_0x3F	00
0x40	Channel 3_0x40	00
0x41	Channel 3_0x41	01
0x42	Channel 3_0x42	04
0x43	Channel 3_0x43	10
0x44	Channel 3_0x44	40
0x45	Channel 3_0x45	08
0x46	Channel 3_0x46	02
0x47	Channel 3_0x47	80
0x48	Channel 3_0x48	03
0x49	Channel 3_0x49	0C
0x4A	Channel 3_0x4A	30
0x4B	Channel 3_0x4B	41
0x4C	Channel 3_0x4C	50
0x4D	Channel 3_0x4D	C0
0x4E	Channel 3_0x4E	60
0x4F	Channel 3_0x4F	90
0x50	Channel 3_0x50	88
0x51	Channel 3_0x51	82
0x52	Channel 3_0x52	A0
0x53	Channel 3_0x53	46
0x54	Channel 3_0x54	52
0x55	Channel 3_0x55	8C
0x56	Channel 3_0x56	B0
0x57	Channel 3_0x57	C8
0x58	Channel 3_0x58	57
0x59	Channel 3_0x59	5D
0x5A	Channel 3_0x5A	69
0x5B	Channel 3_0x5B	75
0x5C	Channel 3_0x5C	D5
0x5D	Channel 3_0x5D	99
0x5E	Channel 3_0x5E	96
0x5F	Channel 3_0x5F	A5
0x60	Channel 3_0x60	00
0x61	Channel 3_0x61	00
0x62	Channel 3_0x62	00
0x63	Channel 3_0x63	00
0x64	Channel 3_0x64	00
0x65	Channel 3_0x65	00
0x66	Channel 3_0x66	00
0x67	Channel 3_0x67	20
0x68	Channel 3_0x68	00
0x69	Channel 3_0x69	0A
0x6A	Channel 3_0x6A	22
0x6B	Channel 3_0x6B	40
0x6C	Channel 3_0x6C	40
0x6D	Channel 3_0x6D	40
0x6E	Channel 3_0x6E	00
0x6F	Channel 3_0x6F	00
0x70	Channel 3_0x70	03
0x71	Channel 3_0x71	00
0x72	Channel 3_0x72	00
0x73	Channel 3_0x73	00
0x74	Channel 3_0x74	00
0x75	Channel 3_0x75	00

  • Hi Megha,

    The DS100DF410 programming guide outlines the correct register sequences for some common device configurations:

    https://www.ti.com/lit/an/snla323/snla323.pdf

    Please try the configuration sequence in Table 9.

    Thank you,

    Evan

  • In addition to Evan's configuration instructions, see below debug suggestions.

    • Make sure that auto-negotiation and link training are disabled on your SOCs at both ends of the link
    • Do confirm that the retimer is achieving CDR lock as part of your system link bring-up. You may check the retimer CDR status via channel register 0x02

    Regards,

    Rodrigo Natal

  • Hi Evan, rodrigo,

    I checked the configuration at our end and then configured the register sequence as per the snla323.pdf [table 9] document. I checked the 0x2f for CDR lock status. It's not locking the CDR. Autonegotiation is disabled at our end and link training is also disabled at our end.

    Please find the i2cdump of retimer device. Please suggest the values.

    -------board1--------CN8350 cavium processor---------

    This board has 3 10G xfi links connected to 3 board2.


    root@debian_on_OCTEON-TX:/home# i2cdump -f -y 0 0x1a

    No size specified (using byte-data access)
         0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef
    00: 00 00 00 00 00 00 00 00 00 00 10 0f 08 00 93 69    ..........???.?i
    10: 3a 20 a0 30 00 10 7a 36 40 23 00 03 24 00 e1 55    : ?0.?z6@#.?$.?U
    20: 00 00 00 40 40 00 00 00 00 00 30 00 72 80 00 c6    ...@@.....0.r?.?
    30: 00 20 11 88 bf 1f 31 00 00 00 00 00 00 00 80 00    . ????1.......?.
    40: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90    .???@?????0AP?`?
    50: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5    ???FR???W]iu????
    60: 00 00 00 00 00 00 00 20 00 0a 44 00 00 00 00 00    ....... .?D.....
    70: 03 20 00 00 00 00 b0 c8 57 5d 69 75 d5 99 96 a5    ? ....??W]iu????
    80: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90    .???@?????0AP?`?
    90: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5    ???FR???W]iu????
    a0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90    .???@?????0AP?`?
    b0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5    ???FR???W]iu????
    c0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90    .???@?????0AP?`?
    d0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5    ???FR???W]iu????
    e0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90    .???@?????0AP?`?
    f0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5    ???FR???W]iu????

    -------board2--------TI-SOC----------

         0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef
    00: 00 10 dc 00 00 00 00 00 00 00 10 0f 08 00 93 69    .??.......???.?i
    10: 3a 20 a0 30 00 10 7a 36 40 23 00 03 24 00 e1 55    : ?0.?z6@#.?$.?U
    20: 00 00 00 40 00 00 00 21 38 20 30 00 72 80 00 c6    ...@...!8 0.r?.?
    30: 00 20 11 88 bf 1f 31 00 10 00 00 00 00 00 80 00    . ????1.?.....?.
    40: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90    .???@?????0AP?`?
    50: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5    ???FR???W]iu????
    60: 00 00 00 00 00 00 00 20 00 0a 44 00 00 00 00 00    ....... .?D.....
    70: 03 20 00 00 00 00 b0 c8 57 5d 69 75 d5 99 96 a5    ? ....??W]iu????
    80: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90    .???@?????0AP?`?
    90: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5    ???FR???W]iu????
    a0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90    .???@?????0AP?`?
    b0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5    ???FR???W]iu????
    c0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90    .???@?????0AP?`?
    d0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5    ???FR???W]iu????
    e0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90    .???@?????0AP?`?
    f0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5    ???FR???W]iu????

  • Hi Megha,

    Could you share a block diagram of the system?

    Board 2 register dump shows CDR locked (0x2[3]) with valid eye measurements (0x27, 0x28).

    Board 1 register values indicate CDR is not locked, with ppm tolerance exceeded and single bit check limit not passed.

    Please confirm the TX signal characteristics for board 1 into the retimer (data rate, pattern, amplitude, de-emphasis settings, ...).

    Also, please try disabling single bit limit check (0xC[3] = 0) to see if this affects CDR lock for board 1.

    Thank you,

    Evan