Part Number: DS250DF410
Other Parts Discussed in Thread: DS560MB410, DS280BR820, , DS250DF230
Hi,
I am current working on a project where I need to have a 25G interface between an FPGA and SFP28 module. The trace length is coming around 7.5 inches with a simulated insertion loss of around 10 dB (using FR408HR material).
Which device is suitable here to use? Redriver is enough or Retimer is required? (I want to use same FR408HR material only for cost reduction)
Can I place the retimer close to the SFP module so that loss towards the SFP side is around 2-3 dB?
Regards,
Sahal