Part Number: PCA9554
Other Parts Discussed in Thread: TCA9554
Hello,
I am using the PCA9554 to drive output enable signals for load switches. All of the IO are configured as outputs at all times and during normal operation, some of the outputs that should be low (0V) are outputting 0.75V-0.815V. This causing load switches to turn on where they should not be. Only 3 of the 8 outputs are exhibiting this behaviour. The outputs that are correctly driven low are measuring 0.08V. All IO pins have 10k external pulldowns. The 3V3 rails looks healthy. Maybe 3 outputs somehow got configured as inputs? The only thing that gets the part out of this state is to full power cycle the 3v3 rail.
Any ideas on what could cause this?
Amy