Part Number: SN65HVD230
Hi, we are using SN65HVD230 for CAN communication. this CAN cable carry +24V which is used to power On other front end device. When GND wire breaks, other device lose it's supply but also this is causing CAN communication failing. when GND re-establish , still problem continue and only way to establish CAN communication is to power cycle main board , where CAN IC is used. How can we re-establish CAN communication without power cycle the main board?