Other Parts Discussed in Thread: TPS25810-Q1, TPS25810
Hi
We need to implement USB type-C for automotive application, I survey the solution are HD3SS3212-Q1+ TPS25810-Q1, however, we need to perform all USB signals+VBUS with "short to VBAT 36V" and "short to GND" testing form ISO 16750-2. Need TI's expert to confirm if both HD3SS3212-Q1 & TPS25810-Q1 support the fault protection ( "short to VBAT 36V" and "short to GND")?
Or we need to add additional protection IC/component?
Regards,
Vincent