Part Number: DP83825I
Hi,
I'm looking for a review of a DP83825i interfaced with a AM6232 processor please.
I've built in some flexibility in terms of clocking and VDDIO setting, as I haven't used this part before with the AM6232. Not shown is the AM62x power pins, however VDDSHV2 will be changed along with the ferrite bead on the PHY VDDIO decoupling.
The default approach is shown and described as option#1 in the config notes.
Questions:
- Is the CLKOUT0/EXT_REFCLK1 50MHz outptu fromthe sitara correctly connected to the PHY and also RMII interface?
- Are there any timing constraints on the 50MHz signals going to the OSCIN of the phy and the RMII_RXC pin?
- The PHY should be slave mode as the external clock can only be set for 50MHz. Is the strapping correct for this?
Please let me know if there are any issues, or changes required.