This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1004: TUSB1004 supports Type C pure USB function

Part Number: TUSB1004
Other Parts Discussed in Thread: TUSB1104, TUSB1044

Hi David, 

Promoted TUSB1104 to customer but customer feedback if they don’t need USB3.2 Gen2 x2 and only have USB 3.2 Gen2 x1 Type-C capability and asked if they can use TUSB1004 in this application if they only have USB 3.2 Gen2(10Gbps) Type C capability without DP Alt mode? Thank you.

Best regards,

Randy