This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

video conversion



Hi, I'd like to ask for components suggestion to realize the following video conversions:

1. DVI--> serial data stream 

2. NTSC --> serial data stream 

3. SDI --> serial data stream 

4. serial data stream --> NTSC

5. serial data stream --> DVI 

Additionally, 6. SDI --> h.264 Ethernet stream

In conclusion, the aim is to serialize three different input video streams (DVI, SDI, NTSC). Each serial stream will be broadcasted into a crosspoint matrix and re-generated into DVI and NTSC. Serial data need to be transmitted on a PCB backplane (e.g. using FDP-linkIII or other serial communication solution) without using cables. Moreover, signals may need to be re-driven before being translated into a serial stream. Additionally, one SDI input has to be converted into an h.264 Ethernet stream.

Thus I would like to ask for your support in suggesting ICs (-EP or at least -40°C to 85°C) to implement the required conversion.

I'd like to thank you in advance for your help.

Best,

VE