Part Number: HD3SS460
Other Parts Discussed in Thread: TMUXHS221,
I want to flip all channels of a USB.3 signals, including digital and analogue signals (0- 3.3V). while I'm using USB. C. differential channels, they are not differential signals. it's not high-speed communication, less than 1G.
I see there is a maximum voltage rating of 2.5V for differential pins, (p.6)
also, in some other MUX products such as TUS1044, although the Max rate for single ended input voltage is 4V, the differential voltage at differential pins is limited to 2.5V.(p.6)
does it mean I cannot use any of this product for transferring digital signals?