This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK10034: use USB-2-MDIO to communicate with TLK10034; Tool detects all PHY IDs and returns FFFF

Part Number: TLK10034
Other Parts Discussed in Thread: MSP430F5529

Hi

I am trying to use USB-2MDIO GUI to talk to TLK10034. The LaunchPad I use is MSP430F5529.

I connect external 1.8V to the MSP430F5529.

When I try to read or write through GUI, it always returns FFFF. 

Plus, when I run the "Find PHY ID" command, it tells that it found on all IDs a working PHY, which is not the case.

Also, one strange thing is that when it runs read/white function and FInd PHY ID, the voltage increases from 1.8V to 2.2V, which not meet the voltage spec for TLK10034(1.8V)

Any help will be appreciated.

Thank you very much!

Duo