Other Parts Discussed in Thread: TCAN4550
Hi team,

Figure 1, yellow for canH signal and blue for spi ncs signal

Figure 2, yellow for the spi ncs signal and blue for the spi SCLK signal
It is thus observed that the can bus signal sends a frame after a spi signal is transmitted. As a result, the module CAN frame interval is up to 1.1 ms.
1, is this normal?
2, can the spi signal content within the frame interval time is necessary to transmit information, is it possible to reduce unnecessary content, so as to achieve the purpose of reducing the frame interval size?
3, does the module work as described above, that is, each CAN frame needs to wait for the spi message containing CAN frame contents to be transmitted before a CAN frame can be issued?
Best Regards,
Amy Luo