Other Parts Discussed in Thread: TCA4307,
Hi I have a design that require the sub-board to be hot swappable, plugin/unplugged while the main-board will operating.
The sub-board is a I2C sensor, the long wire is 2m soldered with sub-board, at the other side is the connector to the main board.
To illustrate relation:
main-board + connector ----i2c---- connector + long wire + sub-board
I see that to support the hot swap, I need to use TCA4307. And from the P82B715 datasheet, I need to have it at both sides.
My question is how the setup should be: