Part Number: DS90UB953-Q1
Other Parts Discussed in Thread: DS90UB954-Q1, ALP
Hi Ti experts,
We're developing a test application to generate a maximum busload on DS90UB954-Q1:
This test app checks whether DS90UB954-Q1 can run with the maximum busload.
I use the camera with: sensor is IMX490, serializer is DS90UB953
So I want to config register for the DS90UB953 pattern generator to generate the max busload to DS90UB954.
Could you provide the set of configuration of registers to the DS90UB953 pattern generator can generate the max busload to DS90UB954
Thank you very much in advance!