I have two different system which has separate VDD and separate GND. I want to communicate between this two systems with CAN. I don't want to use ISO1050 i want to use regular transceiver like SN65HVD232, and i guess this is possible to communicate two systems which have two different ground, just using two line (CAN-H and CAN-L). Because CAN is a differantial base communication.
Am I right?
If i am not, why?
And if i am right, what is the possible problems in this type communication?