Other Parts Discussed in Thread: TCAN334
Hi all,
I am currently using TCAN4550 coupled with an ST controller(STM32F0) for my setup and it is working fine with around 50 nodes on the line.
Recently I have started working with STM32G0 family , and it is having CAN-FD built in with the controller, so I have implemented communication using that separately; using TCAN334GDR transceiver and it is also working fine . What I noticed is that the idle voltage of CAN-H and CAN-L lines in the first case is 2.5V and is around 1.65V in second case (CAN-FD). So, I wanted to know if these are inter-compatible and I can use both of my boards interchangeably or not. If there is any probable issue with this communication or anything I will need to change before trying to do so, please let me know.
Thank you.
Regards
Jayam Srivastava.