Part Number: TUSB8041A
Other Parts Discussed in Thread: TUSB8041,
We are facing a problem with USB HUB TUSB8041 as described:
The crystal oscillator stops working when entering the Windows OS, Could please provide advice for that, thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Zeros:
Where is USB_VBUS connected to? It should be around 0.5v.
Don't know why I can't search in schematic file, can you send a new one I can search ?
Regards
Brian
Zeros:
I didn't see issue in schematic which could cause crystal stop working.
From this waveform , crystal never start working. Is crystal far from HUB device? or any hub soldering issue for ground pad?
Regards
Brian

Hi Brian,
The etch length from crystal to HUB is about 356mils and we can measure crystal working at 24Mhz as below picture,btw,we found the HUB can normal working when re-assert reset signal.

Zeros:
Is that Windows system turn on low power state ( U3) ? It may cause crystal to stop.
Regards
Brian
Hi Brian,
Do you know how to check whether a OS(Windows server 2002) is entring U3 state? btw,We use same OS for another system and didn't find any issues.
HI Brian, we checked the USB HUB crystal also stop at BIOS menu, it didn't related to OS behavior (checked linux and windows also duplicated).
and we tried to re heat chip but still fail, please help to comments if any.
Thanks
Sinden:
let me check with designer what any other reason could cause crystal stop working and update on next Monday.
Regards
Brian
Hi Sinden:
Do you plan to change any setting? default setting itself should work. I can send EERPOM file you need to change anything.
Regards
Brian
Sinden:
"Removing EEPROM" is equivalent to loading default EEPROM. If you need to change anything, then you need to external EEPROM.
Regards
Brian
Sinden:
Please accept my friendship request and I can send EEPROM tool to you.
By the way, what did you change your original EEPROM file?
Regards
Brian
Hi Brian
We would like to know about Bit 2 of register 0A more detail information,could please provide a detailed explanation of the DSPORT ECR(Does it mean 'Error Correction Register'?) enable mechanism and its operation and Is the abnormal operation of TUSB8041 related to this bit?
Thanks.
Zeros:
ECR means Engineering Change Request.
For this ECR, if it was disabled, downstream port will stop reporting port status, so I don't think it will cause the abnormal operation.
Please check bit 5 of 0x05 to see if U1/U2 is disabled or not.
Regards
Brian
Zeros:
Did you try TI EEPROM tool and find any register related?
Regards
Brian
Hi Brian,
Yes, but we encountered another problem when loading the indicated driver for EEPROM tool, which caused all of the HUBs to stop working, and then the mouse and keyboard shut down,So we are looking for a PCIe to USB card to resume mouse and keyboard functions.
Hi Zeros:
You are right, EEPROM tool driver will disable all USB ports on the same root hub and you need PCIe to USB card to control mouse and keyboard.
After exit from EERPOM tool, you need to reboot the system to make hub work as normal.
Please keep update if you make progress
Regards
Brian
Hi Zeros:
I will close this ticket since no update from Mitac.
Regards
Brian
Hi Brian,
OK, by the way, we didn't have the adapter to verify the TUSB8041A firmware, so in the solution part, we removed the flash to ensure that both types of flash can operate normally. Thanks for your support