Dear TI support team,
I was looking through the catalog of products in the website to try and find a DPI to LVDS converter. So far I haven't been able to find one, hence trying to confirm it on here.
Thank you in advance,
Nuri
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI support team,
I was looking through the catalog of products in the website to try and find a DPI to LVDS converter. So far I haven't been able to find one, hence trying to confirm it on here.
Thank you in advance,
Nuri
Nuri,
We have many products in our portfolio which can perform this conversion actually. Can you give more detailed requirements so that I can direct you to the best fit?
- What PCLK rate do you need?
- What temp range do you need?
- Do you need an automotive qualified solution or not?
- What I/O level do you need? 1.8V or 3.3V?
Best Regards,
Casey
Hello Casey,
I appreciate the quick feedback!
- What PCLK rate do you need? I'm looking for products ranging from 35MP/s to 135MP. It's not a set value yet, hence why I was asking for the family of products for such purpose.
- What temp range do you need? -40 to 105 preferentially.
- Do you need an automotive qualified solution or not? Automotive would be preferred.
- What I/O level do you need? 1.8V or 3.3V? It would be great if I can see options for both levels.
Thank you for the support,
Nuri
Nuri,
If you can use -40-85C temp range then SN65LVDS93A-Q1 could be a good option too. That one supports all the way to 135MHz PCLK with 4 lane LVDS output. It can support 1.8V or 3.3V I/O. It has automotive qual as well.
Another popular option for you may be DS90C189-Q1. This device can support:
- Automotive Qual
- -40-105C temp range
- 1.8V I/O
I can support either single LVDS 4 lane output, or dual 4 lane output. In single mode it can support PCLK from 25-105MHz. In dual lane it can support 50-185MHz
Most LVDS applications above ~105MHz use dual mode (2x 4 lane).
Best Regards,
Casey