Other Parts Discussed in Thread: XIO2001, XIO2000A, XIO2001EVM
Hi,
my customer plans to use XIO2001, but now they have production based on XIO2000. And the ask for errata for this device, which was removed from the WEB. Could you help somehow?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: XIO2001, XIO2000A, XIO2001EVM
Hi,
my customer plans to use XIO2001, but now they have production based on XIO2000. And the ask for errata for this device, which was removed from the WEB. Could you help somehow?
Hi,
If you are going to use the XIO2001, then you don't need the errata for the XIO2000.
You can find the XIO2001's errata on the following link:
http://www.ti.com/lit/er/scpz008/scpz008.pdf
Also, there is a transition document from XIO2000 to XIO2001 in the below link:
http://focus.ti.com/analog/docs/litabsmultiplefilelist.tsp?literatureNumber=scpa046&docCategoryId=1&familyId=729
Regards.
Elias,
thank you for reply, but we have a stock of XIO2000 in our warehouse that is prepared for production. We need to use them in this quarter and then we'll switch to XIO2001. For this we need full documentation on XIO2000.
Can these docs fully help?
Hello Dmitry,
It is a very old device but I did find some errata documents.
See attachements.
Regards.
Ellias,
thank you again for your support, the customer says that this is what they need but for the part XIO2000A. Unfortunately, the errata for the A-ver. also was removed. Can you help us again?
Anyway, we have ordered the XIO2001EVM for tests, hope that as soon as they run out of stock they'll start to use the latest part.