This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH1297: SPI ready time is needed?

Part Number: LMH1297

Hello,
There is  SM Bus ready time after POR in the datasheet. How about SPI?

I'm using SPI interface. After 40ms from POR, I initiate device initialization through SPI, but not reflected in LMH1297.

After 100ms from POR, it works well.
Is there any restriction in SPI ready time?

Best Regards,

Murai