Part Number: DS125BR401
Team,
Customer is trying to tune in the downstream direction (PC to EP, as described in section 9.5.1 of datasheet SNLS419D) for a PCI system.
The DS125BR401 sits on a custom PCI add-on card in a PC and is connected through Molex connector via a 50cm cable to a PCI gen 2 end point .
The add-on card is very simple. The 3.3V is coming from the PCI bus. The schematics and PCB guideline from datasheet have been followed.
Enumeration works ok for PCI gen 1, but it is not stable for PCI Gen 2.
SNLS419D Section 9.5.1 mentions PCI Gen 3.
-Is a different configuration/programming required for PCI Gen 2?
-What status register should be read in order to understand better the issue?
-How to debug further this issue?
Thanks in advance,
Anber