Part Number: SN65MLVD206
Hello,
In a harsh industrial environment I am having problems with a M-LVDS communication where the signals shared between transmitter and
receiver are A,B and GND.
In AN-1926 states the following:
"System designers building M-LVDS interfaces over long cables need to ensure that the ground
noise does not exceed the ±1V limit or they need to fully eliminate the DC component of signals by implementing
either AC-coupled or transformer-coupled interfaces".
It occurred to me that I might have this problem.
Most solutions I've found is an ac coupled transmitter with a dc bias receiver.
But I am not sure if this can be done in a half duplex configuration.
Is it possilble to use an ac coupled solution in a half duplex M-LVDS configuration where tx and receiver
lines are shared ?
Regards,
Aitor