This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB962-Q1: 962 related issues

Part Number: DS90UB962-Q1

1,Can the setting of the 962 mode pin be modified again through I2C after power on.

2: What is the maximum bandwidth supported by 962 LANE for 3G?

3: The current MODE setting is RAW10, with a camera of 1920 * 1440, 30fps, and YUV422-8. Can you help confirm whether it is supported (including calculation methods) in terms of bandwidth and PCLK.

  • Hello Ray,

    1,Can the setting of the 962 mode pin be modified again through I2C after power on.

    Yes, in reg 0x6D

    2: What is the maximum bandwidth supported by 962 LANE for 3G?

    Max supported bandwidth at the CSI TX is 1.664Gbps per lane. Keep in mind there is ~ 25% CSI overhead.

    3: The current MODE setting is RAW10, with a camera of 1920 * 1440, 30fps, and YUV422-8. Can you help confirm whether it is supported (including calculation methods) in terms of bandwidth and PCLK.

    Total bandwidth = Hres x Vres x Fps x blanking x #bits/pixle

                              = 1920 x 1440 x 30 x 1.25 x 10 = 1.659 Gbps