Part Number: DS90UB953-Q1
I have a one lane sensor connected to serializer ub953. sensor device is detected and probed successfully. Even I was able to capture frames from it a few days back.
but when I tried again recently with same setup, same driver and device tree configuration. I am able to run gstreamer pipeline to capture video from it but there is no video.
dmesg error:
tegra194-vi5 15c10000.vi: uncorr_err: request timed out after 2500 ms
tegra194-vi5 15c10000.vi: err_rec: attempting to reset the capture channel
t194-nvcsi 15a00000.nvcsi: PH_CHK_CTRL = 0
t194-nvcsi 15a00000.nvcsi: PH_CHK_CTRL = 0
tegra194-vi5 15c10000.vi: err_rec: successfully reset the capture channel
ub953 status registers address and values respectively are as follows
ub953 register 0x02, value=43
ub953 register 0x03, value=48
0x04, value=00
0x05, value=03
0x06, value=41
0x07, value=28
0x32, value=09
0x50, value=20
0x51, value=c0
0x52, value=65
0x55, value=00
0x56, value=00
0x5b, value=02
0x5c, value=ff
0x5d, value=0f
0x5e, value=0c
0x5f, value=00
0x60, value=00
0x61, value=ff
Waiting for data vc... (VC=3, Data ID=3f)
0x62, value=09
0x63, value=00
0x64, value=80