This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD2410V: Internal circuit for hot plug-in and failsafe

Part Number: THVD2410V
Other Parts Discussed in Thread: THVD2410

Hi,

The first page of the datasheet lists “Glitch-free power-up/down for hot plug-in capability” and“ Open, short, and idle bus failsafe.”

1) Could you tell me the detailed internal circuit for hot plug-in?

2) Could you tell me the detailed internal circuit for failsafe?

Best Regards,

Nishie

  • Hi Nishie,

    I can't give you the internal circuits of our devices - its our IP so we don't share that outside of TI. 

    I can give you a high level description of how it works - which is really all you need to design with the part. 

    1) The glitch free power-up and power-down for hot plug  applications means that if the driver and receiver are disabled during power up you won't have a glitch. By default DE is pulled low and /RE is pulled high internally to the device - which means by default the device is disabled so during power up / power down that you would see in power-up and power down. The caveat on this device is that it is assumed that VIO is active during the hotplug because there is a direct connection from logic inputs to VIO - if this is unwanted than the THVD2410 is the better option because essentially it removes the VIO supply - the VIO supply is what causes this caveat to be mentioned. 

    2) The receiver fail-safe on this device is timer based. Meaning if the input differential voltage is between -40mV and 40mV for t(OFS) then the receiver will output a high -during idle/open/short VID = 0V - so that time period is how long it takes to enter a fail-safe state. The value of t(OFS) depends on the state of SLR pin in the application as it does impact the delay value - this is listed in the switching characteristics of the receiver in the datasheet.  How this works in practice is if for example you are transmitting a logic low when a fail event occurs - lets say a short - the VID will go from < -200mV to 0V at this time the "R" pin will be continue outputting a "low" signal - if the VID remains between -40mV and 40mV for t(OFS) the "R" pin will then output a logic high and will continue until it leaves the -40mV to 40mV range and if t(FSO) has passed the "R" pin will follow VID input - please note that t(FSO) is different than t(OFS) - both listed in the same section of datasheet. 

    Best,

    Parker Dodson

  • Hi Parker-san,

    Thank you for your detailed explanation. I understand that the internal circuit is IP.

    I have additional question.

    Is the description about the plug-in different from the protection against the operation when hot swapping of the D-sub of the 9 pin?

    I thought the hot plug-in capability function works when inserting/removing the D-sub of the 9pin. However, I thought that the insertion/removal of the A/B/Z/Y pins (data) occurs in the D-sub, but the insertion/removal of the power supply does not occur.

    Best Regards,

    Nishie

  • Hi Nishie,

    So hot plug can refer to the module being placed into a live backplane or it could include plugging an active RS-485 bus to an unpowered device. 

    I believe your question is focusing on the second side - when just data is sent to an unpowered RS-485 device - in that case the RS-485 bus by standard has to be able to handle -7V to 12V inputs - and that is regardless of VCC state. So the RS-485 bus as required by standard is hot pluggable by that definition. This device specifically can handle up to -70V to 70V regardless of VCC state. I apologize I didn't make that clearer - but teh RS-485 bus pins are already hot-pluggable due to how the bus facing pins need to be designed. You may see a slightly different loading from these pins when VCC = 0V because an internal bias network is turned off without VCC, but ultimately it is hot-pluggable in that sense. 

    Best,

    Parker Dodson

  • Hi Parker-san,

    Thank you for your support.

    Regarding RS232, is it possible for you to answer? The contents are as follows.

    Please tell me an example of an external circuit when the IC of RS232 is used for hot-swap. Surge protection diode, insulation, etc.

    I understand that RS232 does not support hot-swap.

    Best Regards,

    Nishie

  • RS-232 uses point-to-point connections, so it does not need to care about any ongoing communication while (un)plugging.

    RS-232 receivers must be able to tolerate ±25 V. You should already have ESD and surge protection, depending on your environment; this will be enough to allow hotplugging.

  • Hi Nishie,

    Clemens is correct. 

    Best,

    Parker Dodson