Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD4E02B04-Q1: Usage of S-Parameter in Circuit simulation

Part Number: TPD4E02B04-Q1

Hi TI team.

We would like to perform waveform verification in a circuit simulator using the S-parameter of TPD4E02B04-Q1.

(The S-parameter can be obtained from https://www.ti.com/jp/lit/zip/slvmbk1)

1. It appears that the S-parameter of TPD4E02B04-Q1 are based on actual measurement data.

Are the wiring and pads de-embedded?

2. We plan to obtain the S-parameters of the PCB through electromagnetic simulation.

The correspondence between the wiring and the ports is as shown in the diagram.

In this case, we believe the connection between the S-parameters of TPD4E02B04-Q1 and the PCB is as follows:

PCB Port2 -> TPD4E02B04-Q1 Port1

PCB Port3 -> TPD4E02B04-Q1 Port3

PCB Port6 -> TPD4E02B04-Q1 Port2

PCB Port7 -> TPD4E02B04-Q1 Port4

Is this correct?

Regards,

Matsumoto