Part Number: TCA9548A
Dear Team,
In our system, TCA9548 is used in the following order:
Power-up reset pulls reset pin
Write command to select channel 1 – > 0x02
Operate the I2C device behind mux
Write command 0x00 to close all channels when the operation is complete.
Return to step 2.
During this continuous operation, we found that in step2, communication errors often occur on the mux I2C input port, sometimes the SCL is lost. Sometimes the data on SDA is incorrect. The reason is unknown.
if our processes are reasonable and if there is room for further optimization. Thank you!