Part Number: TUSB1142
Hello,
We have questions about Table 10-1. Design Parameters on TUSB1142 datasheet SLLSFL2.
- "Minimum distance of the AC capacitors from TUSB1142, LAC-CAP : 0.4 inches"
What is reason of minimum pattern length 0.4 inches requirement between PIN to CAP terminal inside of 2 inches <= XAB, <= 12 inches - XCD ?
Is that considering of impedance matching or something?
- "CAC-USB1 AC-coupling capacitor (75 nF to 265 nF)" "CAC-USB2 AC-coupling capacitor (297 nF to 363 nF)"
Those CAPs are purposing just DC blocking, but why it have such a narrow acceptable tolerance?
What is problem if we use larger CAP like 470nF?
Regards,
Mochizuki