This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8044AEVM: TUSB8044A

Part Number: TUSB8044AEVM
Other Parts Discussed in Thread: TUSB8044A,

Hello,

My name is Pavel Skoda - I am going to design the USB-C HUB with TUSB8044A (I need 2x USB 2.0 outputs and 1x HDMI output) - I am planning to use the Eval board for preliminary test. 

According to data sheet the TUSB8044A is USB 3.2 Gen but:

1. Why the TUSB8044AEVM is USB 3.0 (per Digikey description)? Can I change it to 3.1 (or 3.2)?

2. I would like to use on one of the downstream output the HDMI (V 1.4) connector for LCD 1280x800 resolution. Is the GPU required for that output or the TUSB8844A is capable to deliver video data?

3.  Is there any other suggestion for that kind of design?

Thank you for your help.

Pavel