This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB8041A: TUSB

Part Number: TUSB8041A
Other Parts Discussed in Thread: TUSB1210

Hi team,

do we have device to support universal interface chip for the USB bus, it supports USB-HOST host mode and USB-DEVICE/SLAVE device mode. It has a built-in 3-port HUB root hub and supports low-speed and full-speed control transmission, batch transmission, interrupt transmission, and synchronous/isochronous transmission.
Description of key parameter requirements: Working voltage: -0.5~6.0v; Bus protocol: SPI to USB; Communication speed: 6MB speed 8-bit passive parallel interface and 3.5MB/28MHz speed SPI serial interface;