Other Parts Discussed in Thread: MAX3221
The hardware configuration is below .Normal mode operation (As per datasheet)
We are facing a problem related with MAX3221 RS 232 communication chip.
The chip is not properly work with communication port of PC. Here I have selected the communication port as default settings (baud rate=9600, data bit= 8, parity= none, stop bit= 1).Also tried with up to 57600 different bauds but no response.
The same hardware & PC settings are worked with (Prolific USB to COM port converter).
So I was doubt on COM port & checked the port by shorting of TX& RX Pin of port & tested with HyperTerminal (loopback).The PC’s port was working properly.
As per datasheet Data rate is
The min value of data rate is 150kbps. So whether it is working with baud rate 9600 to 57600?