Other Parts Discussed in Thread: SN75DP139, TFP410
Hello,
Does the SN75DP128A handle R,G,B, CLK data types. I read this device is DP 1.1a only. Is this correct? From what I read, this does not support R,G,B data application. I'm looking to build a dual DP graphics path to support 2560x1600 at 60Hz to Dual Link DVI output. Is there an application note about this possible configuration.
One possible method I'm wondering about is the SN75DP128A demux driving two separate SN75DP139 translators to create the two separate R,G,B, CLK signal sets for DVI dual link connector. I'm wondering if this is possible to build and keep the skew low enough.
thank you