Part Number: DS125DF1610EVM
Other Parts Discussed in Thread: DS125DF1610
I am trying to set up the loopback test to verify the BERT feature of DS125DF1610EVM. But I am having difficulty to make it work. I wonder if there is any reference guide to do this loopback test. Below are the steps I have done:
1) I powered up the EVM board and connected it PC with USB and loaded the configuration for DS125DF1610. SIgCon Arch shows the board is connected. REF_CLK is set to 312.5 MHz.
2) Use SMA2SMA cables to Connect TX_4A_P/N to RX_4B_P/N.
3) On SigCon Arch, at channel select, select RX/TX_4A, then go to PRBS Gen/Checker tab, select PRBS31 then click Enable. click "apply to channel"
4) The channel indicators shows "No signal", "CDR unlocked"
It seems like the PRBS31 is not generated for TX_4A ports. and also not detected on RX_4B ports.
I also did another test. Use SMA2SMA cables to connect TX_4A_P/N to RX_4A_P/N (instead of RX_4B_P/N). Then enabled the PRBS31 on RX/TX_4A. I can see "signal detected". But I cannot get CDR to lock. Also on the user guide, it states "the PRBS generator and PRBS checker should be operated from different channels". I am really confused on how to set this loopback test.
Best,
Wendy