Part Number: SN75175
Other Parts Discussed in Thread: AM26C32, AM26LV32
Hi,
We are looking at the SN75175 for a product that will receive either or a RS422 or single ended TTL (5V.) We will need to handle either option on the same input port/pins. It would need to be for 3 differential encoder inputs.(A,B,Z) Would using the 1A,2A,3A be able to receive a single ended TTL?
Is there another Receiver option that may be more suitable for this?
Best regards
LC