Part Number: SN75LVDS83B
Hi team,
1. If the 10% to 90% rise or fall time is greater than 3 ns, how is the input timing defined?
2. What will be the impact if the 10% to 90% rise or fall time is greater than 3 ns?

Thanks
Lillian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN75LVDS83B
Hi team,
1. If the 10% to 90% rise or fall time is greater than 3 ns, how is the input timing defined?
2. What will be the impact if the 10% to 90% rise or fall time is greater than 3 ns?

Thanks
Lillian
Hi Lillian,
The datasheet "7.7 Timing Requirements" section's "Input signal transition time" is maximum 3ns, so the incoming signals should meet that criterion.
Is there any issue with meeting the rising/ falling edge requirements?
Best regards,
Ikram