Tool/software:
Figure 7-1 from the datasheet shows VDDIO becoming stable before VAVD begins to rise. The T1 number from the 7.6 Table, says that it can be +/- 100mS. Which means that VAVD could power up before VDDIO, or they can power up at the same time. However note number three states: "AVD ramping up AFTER VDDIO ramp completion is preferred to avoid false detection of lower level VDDIO in any corner case". What exactly does that mean?
I've checked the DP83822 Schematic Checklist and there is no mention of making sure VAVD ramps after VDDIO. I've checked the EVM schematic, and VAVD and VDDIO ramp at the same time. Basically outside of this note #3 from Table 7.6, and can see no effort on TI's part to follow this guidance. Therefore, is it required? Helpful? Not needed? Other? Please explain.
Thanks, Dean