This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS160PR1601: why this part need 50ms before it can be read/write by I2C,

Part Number: DS160PR1601


Tool/software:

Hi experts,

I'm using ds160pr1601 in my PCIE path to boost PCIE signals for PCIE3.0 x8, and my board is installed in a PC.

in 20% of cases, 4 boards can only be recognized as GEN3 x2 at cold boot , after reboot they can link up to GEN3 x8; In 80% of cases they can link up to GEN3 x8 

I got 2 quesitons:

Q1,  I'm using a MCU to control I2C bus, but I can only get ACK after about 50ms, otherwise I can only get NACK, can you tell me why?

Q2, once configuration is done, will this re-driver function immediately,  or it has to wait some time? If so, how long will it take?

Regards

Chris

  • Hi Chris,

    Thank you for reaching out about these questions.

    1. Please see data sheet section 6.7 regarding SMBus/I2C timing characteristics, field T_POR: https://www.ti.com/document-viewer/DS160PR1601/datasheet#GUID-XXXXXXXX-SF0T-XXXX-XXXX-000000317136/GUID-XXXXXXXX-SF0L-XXXX-XXXX-000000317136 
    2. The redriver will function immediately after ALL_DONE_N is asserted low in SMBus Primary/EEPROM mode, or immediately after POR in SMBUs Secondary Mode. When PDx pins are asserted low, the channels associated with each PDx pin will power on and triggers the PCIe RX Detect state machine.

    Do you know when the PDx pins are being asserted and if the PCIe Reset (PERST#) signal is de-asserted after redriver configuration is complete?

    Best,
    David

  • Hi David,

    Thanks for your quick response.

    For 1, I programmed DS160PR1601 directly, so I was wondering it might be different from EEPROM Timing, in which the TPOR is 50ms.

    For 2, in my case, PDx are always being de-asserted, I found it should be toggled in Table 7-1 of datasheet, I can have a try and let you know. Fortunately I have some backup plane in my circuit. 

    What's the desired timing between PDx, PERST# and configuration? If PDx should be inverted of PERST#, can I still be able to do configuration during PDx is asserted.

    What if I set RX detect control register (offset 0x04) to 0x04, so it will continue doing Rx detect?  Any suggestion?

    Regards

    Chris

  • Hi Chris,

    T_POR holds true for both SMBus/I2C modes.

    Configuration of the redriver should be done before PERST# is de-asserted - as the EQ settings of the redriver will impact the signal integrity of the channels of the PCIe link. If PDx pins are tied to inverted PERST#, then this timing holds true. If toggling PDx pins manually, SMBus configuration should be done before toggling PDx pins low.

    EQ setting configuration can be done while PDx pins are high.

    Setting channel RX Detect register 0x04 = 0x04 will override the RX Detect block of the redriver. This would not continue performing RX Detect.

    Best,
    David

  • Hi David,

    Thanks for helping.

    I think this issue is very clear, I'll move forward with inverted PERST# to control PDx. Bypass RX Detect is not a expected behavior for a re-driver.

    Regards

    Chris