Part Number: HD3SS214
Other Parts Discussed in Thread: TMUXHS4612
Tool/software:
Hi,
Does TI have DP2.1 passtive mux as HD3SS214?
Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: HD3SS214
Other Parts Discussed in Thread: TMUXHS4612
Tool/software:
Hi,
Does TI have DP2.1 passtive mux as HD3SS214?
Thanks!
Jeff
Jeff
We are planning to release TMUXHS4612 this year which will support DP2.1 UHBR20.
Thanks
David
Hi,
May I know it can using HW select? or it need I2C control?
Other schedule quesiton I will ask in email.
Thanks!
Jeff
Jeff
The MUX is controlled by HW select, it does not have I2C control.
Thanks
David
Hi David,
If we needs using HD3SS214 first come, first served. Need to auto detect plug and unplug if connected simultaneously. Currently prioritize hardware control display without going through FW.
Is it possible to achevice? or we needs SoC send GPIO to control aux_sel and dx-sel?
Thanks!
Jeff
Hey Jeff,
What speed of DP2.1 are you planning to use? The HD3SS214 only goes up to HBR3 (8.1 Gbps). If you are looking to do autodetect for plug and unplug, the HPD signal can be monitored to determine where a sink is plugged in. What can be done is connect HPD for channel A to the AUX_SEL and DX_SEL pins. This means when HPD is plugged in on channel A, data and aux will be sent across channel A. When channel A is not connected the default routing will be to channel B. However if both channel A and channel B are plugged in only channel A will receive data.
Its better to use firmware to ensure logic is correctly done, and there is a good failsafe mechanism.
Hi Vishesh,
We only support below 8.1Gbps, we have tried it can work with manual select input channel.
Since our SOC can not support FW control, if using HPD with some logic schematic.
If port-1 plug in show port-1, after port-2 plug in, switch to port-2.
Do you have any reference design for this?
Thanks!
Jeff