This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK110: TLK110PT fails to autonegotiate above 50 deg C

Part Number: TLK110

Tool/software:

I am picking up on an issue with the TLK110PT phy chip that seems to align well with the following problem report: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/647280/tlk110-half-of-the-devices-unresponsive-above-70-degrees-c?tisearch=e2e-sitesearch&keymatch=TLK110#.  What was the resolution for this customer?
Failure mode;
  • When the unit reaches thermal equilibrium with the oven ambient temperature above approx 50 deg C, it is no longer able to auto-negotiate a physical link with a remote partner outside the oven (also with a TLK110 phy).
  • If the unit is powered and allowed to negotiate the link at a lower temperature, it remains connected up to (and beyond) the board maximum ambient temperature of 70 deg C.
  • Similarly, if the unit starts up in the failed mode at an ambient above 50 deg C, it does not renegotiate when the temperature is reduced to normal room temperature.
  • Behaviour when physically unplugging the link is indistinguishable from a power up (failure assumed to occur in part of the early negotiation).
  • When the unit is unpowered but connected, the partner link light flashes slowly (0.5Hz).  
Configuration;
  • We are bringing up the unit in hardware bootstrap mode, therefore we believe there to be no reliance on software/initialisation to establish the physical link.
  • Both the unit under test and the link partner are expected to auto-negotiate the link parameters.
What we have tried;
  • We have tried, and eliminated, the recommended advice in the above forum post of pulling JTAG_TDI high via a 1.5K pull-up.  Are TI aware of a feature, documented or otherwise, whereby the part may get stuck in JTAG mode above a certain temperature?
  • Additionally, the following problem report was raised by a departed colleague on a related product: https://e2e.ti.com/support/interface-group/interface/f/interface-forum/840325/tlk110-power-on-issue-with-tlk-110
  • Bob Grice's reports suggest a working-fail-working 'window' whereby MDIO comms also fails, my current problem is more of a working-fail 'threshold' where MDIO continues to respond.  I do not believe it to be the same problem at the present time.
  • Nonetheless, following the advice in Bob Grice's problem report we have reverified the following;
    • We have checked the input clock, which is generated by a crystal osc and forwarded via a clock buffer, both are within specification.  We are able to see RX_CLK, rate appears to be correct.
    • We have increased the ramp-rate for the 3V3 rail to 47us.
    • We are still unable to ensure the clock circuits are powered and stable before applying power to the TLK110.
    • None of the above has resolved the issue at temperature.
Other points to note;
  • When the unit fails to negotiate the link after starting up above 50 deg C, the MDIO interface remains functional.  A software reset does not cause the link to be re-established.
  • If a valid link partner is replaced by an external loopback plug (TX -> RX), a previously failing unit is able to establish a link with itself regardless of temperature.  Are TI aware of any issues with internal clocks moving out of tolerance at temperature? 
  • Failing units have been identified from the following suppliers with the following TLK110 date codes (all suppliers have provided a C-of-C);
    • Mouser (TI date-code 1927, Texas? [Perhaps generic country-of-origin] )
    • Rebound (TI date-code 1849, Thailand)
    • Arrow (TI date-code 2228, Taiwan)
  • Are TI aware of any thermal-related issues with TLK110 parts from the above date-codes/fab plants?
  • Hello,

    Thank you for the information. I would like to caution that TLK110 is NRND, and support is sparse and is limited to datasheet. Is it possible to conduct a register dump (all registers) for the following cases:

    - DUT linked up below 50C

    - DUT linked up and then temperature ramped above 50C

    - DUT link down below 50C

    - DUT linked down due to being powered on above 50C

    Could you also please share our schematics so we can do a quick check on the design if there is any marginal that is contributing to this behavior?

    Sincerely,

    Gerome

  • Hi Gerome,

    Thank you for your rapid response.  Please can you furnish me with a support email address for delivery of the requested schematic sheet and the register dumps.

    Many thanks.

    All best,

    Chris.  

  • Hi Chris,

    Can you please contact your local TI field contact? We can handle communication regarding schematic via this avenue.

    Sincerely,

    Gerome

  • Hi Gerome,

    I forwarded the requested data to you in a PM on 09/08/24, please can you confirm receipt and a likely initial feedback timescale.

    Issues remain ongoing.

    All best,

    Chris.

  • Hi Chris,

    Looks like E2E never gave me a notification of receipt, but looks like its there. My apologies for the delay. Allow me to take a look a the files and analyze. I expect a response by EoW.

    Sincerely,

    Gerome

  • Hi Gerome,

    I suspected it would be something like that.  Not to worry, I'll look forward to your assessment in due course.

    All best,

    Chris.

  • Thank you for your patience.

  • Hi Chris,

    I see in some logs Reg 0x17 differ on [5]. This would be a difference in RMII vs MII and would have functional affect. I would suggest investigating more into this as the register availability on this device is limited compared to those in our modern portfolio. Aside from that, there isn't much else I can spot on registers. As the design work with some sensitivity to temperature, I would expect to determine much from schematic.

    Sincerely,

    Gerome

  • Hi Gerome,

    Many thanks for your kind support in reaching a resolution to this issue.

    All best,

    Chris.