Tool/software:
We are using the DP83867E in combination with the Zynq Ultrascale+.
The interface we are using is SGMII, and there are no issues with normal communication.
However, when we apply static electricity, the link is lost, and the value at PHY address 0x0013 appears to be 0x0504 at that time.
We suspect an SGMII error and observed the SGMII signals with an oscilloscope.
The differential amplitude of the output from the Zynq was around 600mV, whereas for the DP83867E, it was about 300mV or less.
Is there a way to increase the amplitude of the SGMII output from the DP83867E?