This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
◆Question
Is it okay to use this circuit for unused ports?
(Does it need to be connected to VCCI or GND?)
In Table 5-1. Pin Functions, it is set as an input at power up.
Best regards
Hi User,
Best practice is to tied unused pins configured as INPUTs to either VCCP or GND through a resistor.
Otherwise, you can also configure these floating pins on power up to floating OUTPUTs.
If you leave them floating, there is a chance that the device will power up with an interrupt asserted because the voltage on the input is floating and subject to change.
Regards,
Tyler