This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TCAL9539-Q1: What I2C IO Expanders Support Q1 Grade?



FAQ: Logic and Voltage Translation >  IxC >> What I2C IO Expanders Support Automotive Grade 1?  

There are a total of 3 to date. 

TCAL9539-Q1 - 16-bit, 1.08V to 3.6V I2C IO Expander, single supply, interrupt, reset, Agile I/O Configuration

TCA6408A-Q1 - 8-bit 1.65V to 3.6V I2C IO Expander, dual supply, interrupt, reset, and config registers

TCA9539-Q1 - 16-bit, 1.65V to 3.6V I2C IO Expander, single supply, interrupt, reset, and config registers