Other Parts Discussed in Thread: DS280MB810
Tool/software:
Hi,
In addition to the Re-Driver capability of the DS560MB410, it can also perform as Mux.
in our application we want to use this Re-Driver in addition to its driving function as a MUX between 2 types of signals, NRZ and PAM4.
both signals are 12GHz and we want to change the cross point during data communication.
We have two questions regarding the above:
- Is this possible on the fly using one or more of the MUXSEL IO’s or do we have to perform this cross only with channel register change?
- Also what is the speed of the transition between lanes?
The Turn-ON time (SEL to Output) and Turn-OFF time (SEL to Output).
below block diagram concept: