Other Parts Discussed in Thread: TL16C754C
Hi,
We are using TL16CP754CIPM from Texas Instruments.
We have some observations which are different from as described in UART controller datasheet.
- We want to have a Modem Interrupt. To enable this IER[3] is set to 1. I can see that INTA ping being toggled. But, when we read on this pin going high IIR shows a value of 0x1, which means there is no interrupt.
- Can you please clarify what is the value for IIR[5:0] when modem interrupt is generated. In TI's data sheet it shows a value of 0x8 but when we see the exar datasheet part number (ST16C654) it shows a value of 0x0. Please clarify this
- MSR[4] shows a value of zero when /CTS is low and a value of 1 when /CTS is High
- Similarly to make /RTS low we have to write a value of 0 and a value of 1 to make it high which contradicts with the description given against it.
Please help us in understading it.
Regards,
GSR