Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: DS90UB953-Q1,
Tool/software:
Hi Team,
I have used the part DS90UB954-Q1 De-Serializer in my board and with DS90UB953-Q1 Combinations in Camera Module. One of my board iam facing video streaming issue ,MIPI output is not coming from the Deserializer. When connecting the same camera to the other board video stream getting properly. One particular board having issue with DS90UB954-Q1 De-Serializer. The configurations we are applying are same for both working board and Non working board. Pease refer the below register status read out from both boards. In Non working board it seems CSI disabled (With 0x33 status read) . Is there any internal diagnostics making this CSI disable? Can you please guide me for further debug.
We are only using one port RX0.
| Register Address DS90UB954-Q1 |
Non Working Board | working board | Remarks |
| 0x04 | 0xdf | 0xdf | TRUE |
| 0x05 | 0x01 | 0x01 | TRUE |
| 0x06 | 0x00 | 0x00 | TRUE |
| 0x4D | 0x13 | 0x13 | TRUE |
| 0x4E | 0x04 | 0x6d | FALSE |
| 0x55 | 0x00 | 0x00 | TRUE |
| 0x56 | 0x00 | 0x00 | TRUE |
| 0x57 | 0x00 | 0x00 | TRUE |
| 0x7A | 0x00 | 0x00 | TRUE |
| 0x7B | 0x00 | 0x00 | TRUE |
| 0xB9 | 0x33 | 0x33 | TRUE |
| 0xD0 | 0x00 | 0x00 | TRUE |
| 0x24 | 0x00 | 0x00 | TRUE |
| 0x36 | 0x00 | 0x00 | TRUE |
| 0x37 | 0x00 | 0x00 | TRUE |
| 0x35 | 0x00 | 0x01 | FALSE |
| 0x73 | 0x00 | 0x05 | FALSE |
| 0x74 | 0x00 | 0x14 | FALSE |
| 0x75 | 0x00 | 0x06 | FALSE |
| 0x7C | 0x20 | 0x20 | TRUE |
| 0x7D | 0x00 | 0x00 | TRUE |
| 0xB3 | 0x00 | 0x08 | FALSE |
| 0x6D | 0x78 | 0x7c | FALSE |
| 0xB8 | 0x88 | 0x8c | FALSE |
| 0x33 | 0x00 | 0x01 | FALSE |
Thanks Regards
SHIJU.R