Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: ds90ub948 generate pattern script

Part Number: DS90UB948-Q1

Tool/software:

Hi TI,

we need a scripts that ds90ub948 generate pattern.

Regards,

Zhen

  • Hey Zhen,

    What video timing do you need to generate?

    Regards,
    Fadi A.

  • 1 internal timing and internal pclk

    2 internal timing and external pclk

    3 external timing and external pclk

    Regards,

    Zhen

  • Hey Zhen,

    Can you send me the timing for your display. 

    THW =
    TVW =
    AHW =
    AVW =
    HBP =
    VBP =
    HSW =
    VSW =
    HFP =
    VFP =
    PCLK =
    Bits_per_pixel =

    Regards,
    Fadi A.

  • Parameters are as follows:

    Parameters are as follows(PCLK=91.5MHz):

    THW = 2028
    TVW = 752
    AHW = 1920
    AVW = 720
    HBP = 32
    VBP = 21
    HSW =24
    VSW = 3
    HFP = 52
    VFP = 8
    PCLK = 91.5
    Bits_per_pixel = 24

    Regards,

    Zhen.

  • Hi Zhen,

    I will generate and get back to you within 1-2 business days.

    Regards,
    Fadi A.

  • Hi Zhen,

    Can you try attached script?

    import time
    
    #Patgen with internal timing for this video timing
    # THW = 2028
    # TVW = 752
    # AHW = 1920
    # AVW = 720
    # HBP = 32
    # VBP = 21
    # HSW =24
    # VSW = 3
    # HFP = 52
    # VFP = 8
    # PCLK = 80 Mhz using AON CLk
    
    Des_addr = 0x58 #IDx Strap for 928 I2C Address
    
    time.sleep(0.5)
    board.WriteI2C(Des_addr,0x01,0x02) # Reset (Can comment out --- it's optional) 
    
    
    time.sleep(0.5)
    board.WriteI2C(Des_addr,0x66,0x1A)
    board.WriteI2C(Des_addr,0x67,0x01) #M=1
    board.WriteI2C(Des_addr,0x66,0x03)
    board.WriteI2C(Des_addr,0x67,0x02) #N=2
    
    board.WriteI2C(Des_addr,0x66,0x04)
    board.WriteI2C(Des_addr,0x67,0xEC) #least 8 bit of Total Horizontal frame size
    board.WriteI2C(Des_addr,0x66,0x05)
    board.WriteI2C(Des_addr,0x67,0x07) #Least 4 bit TV + Most 4 bit TH
    board.WriteI2C(Des_addr,0x66,0x06)
    board.WriteI2C(Des_addr,0x67,0x2F) #Most 8 bit of Total Vertical frame size
    
    board.WriteI2C(Des_addr,0x66,0x07)
    board.WriteI2C(Des_addr,0x67,0x80) #least 8 bit of active Horizontal frame size
    board.WriteI2C(Des_addr,0x66,0x08)
    board.WriteI2C(Des_addr,0x67,0x07) #Least 4 bit AV + Most 4 bit AH
    board.WriteI2C(Des_addr,0x66,0x09)
    board.WriteI2C(Des_addr,0x67,0x2D) #Most 8 bit of active Vertical frame size
    
    board.WriteI2C(Des_addr,0x66,0x0A)
    board.WriteI2C(Des_addr,0x67,0x18) #Horizontal Sync Width
    board.WriteI2C(Des_addr,0x66,0x0B)
    board.WriteI2C(Des_addr,0x67,0x03) #Vertical Sync Width
    board.WriteI2C(Des_addr,0x66,0x0C)
    board.WriteI2C(Des_addr,0x67,0x20) #Horizontal back porch
    board.WriteI2C(Des_addr,0x66,0x0D)
    board.WriteI2C(Des_addr,0x67,0x15) #Vertical back porch
    
    board.WriteI2C(Des_addr,0x65,0x04) #using internal timing and internal clock
    board.WriteI2C(Des_addr,0x64,0x15) #enable PG/color bars
    
    
    

    Regards,
    Fadi A.

  • This script doesn't work

    Regards,

    Zhen.

  • Hi Zhen,

    I see the issue. Your PCLK is too high for internal oscillator. 948 can go up to 70 Mhz max frequency for PCLK.

    Are you able to run external PCLK with internal timing? Or external timing with external PCLK? If so, I have both of these scripts attached for you. 

    import time
    
    #Patgen with internal timing for this video timing
    # THW = 2028
    # TVW = 752
    # AHW = 1920
    # AVW = 720
    # HBP = 32
    # VBP = 21
    # HSW =24
    # VSW = 3
    # HFP = 52
    # VFP = 8
    # PCLK = 80 Mhz using AON CLk
    
    Des_addr = 0x58 #IDx Strap for 928 I2C Address
    
    time.sleep(0.5)
    board.WriteI2C(Des_addr,0x01,0x02) # Reset (Can comment out --- it's optional) 
    
    
    time.sleep(0.5)
    board.WriteI2C(Des_addr,0x66,0x1A)
    board.WriteI2C(Des_addr,0x67,0x01) #M=1
    board.WriteI2C(Des_addr,0x66,0x03)
    board.WriteI2C(Des_addr,0x67,0x02) #N=2
    
    board.WriteI2C(Des_addr,0x66,0x04)
    board.WriteI2C(Des_addr,0x67,0xEC) #least 8 bit of Total Horizontal frame size
    board.WriteI2C(Des_addr,0x66,0x05)
    board.WriteI2C(Des_addr,0x67,0x07) #Least 4 bit TV + Most 4 bit TH
    board.WriteI2C(Des_addr,0x66,0x06)
    board.WriteI2C(Des_addr,0x67,0x2F) #Most 8 bit of Total Vertical frame size
    
    board.WriteI2C(Des_addr,0x66,0x07)
    board.WriteI2C(Des_addr,0x67,0x80) #least 8 bit of active Horizontal frame size
    board.WriteI2C(Des_addr,0x66,0x08)
    board.WriteI2C(Des_addr,0x67,0x07) #Least 4 bit AV + Most 4 bit AH
    board.WriteI2C(Des_addr,0x66,0x09)
    board.WriteI2C(Des_addr,0x67,0x2D) #Most 8 bit of active Vertical frame size
    
    board.WriteI2C(Des_addr,0x66,0x0A)
    board.WriteI2C(Des_addr,0x67,0x18) #Horizontal Sync Width
    board.WriteI2C(Des_addr,0x66,0x0B)
    board.WriteI2C(Des_addr,0x67,0x03) #Vertical Sync Width
    board.WriteI2C(Des_addr,0x66,0x0C)
    board.WriteI2C(Des_addr,0x67,0x20) #Horizontal back porch
    board.WriteI2C(Des_addr,0x66,0x0D)
    board.WriteI2C(Des_addr,0x67,0x15) #Vertical back porch
    
    board.WriteI2C(Des_addr,0x65,0x00) #using Ext. Timing/Ext. CLK
    board.WriteI2C(Des_addr,0x64,0x15) #enable PG/color bars
    
    
    
    import time
    
    #Patgen with internal timing for this video timing
    # THW = 2028
    # TVW = 752
    # AHW = 1920
    # AVW = 720
    # HBP = 32
    # VBP = 21
    # HSW =24
    # VSW = 3
    # HFP = 52
    # VFP = 8
    # PCLK = 80 Mhz using AON CLk
    
    Des_addr = 0x58 #IDx Strap for 928 I2C Address
    
    time.sleep(0.5)
    board.WriteI2C(Des_addr,0x01,0x02) # Reset (Can comment out --- it's optional) 
    
    
    time.sleep(0.5)
    board.WriteI2C(Des_addr,0x66,0x1A)
    board.WriteI2C(Des_addr,0x67,0x01) #M=1
    board.WriteI2C(Des_addr,0x66,0x03)
    board.WriteI2C(Des_addr,0x67,0x02) #N=2
    
    board.WriteI2C(Des_addr,0x66,0x04)
    board.WriteI2C(Des_addr,0x67,0xEC) #least 8 bit of Total Horizontal frame size
    board.WriteI2C(Des_addr,0x66,0x05)
    board.WriteI2C(Des_addr,0x67,0x07) #Least 4 bit TV + Most 4 bit TH
    board.WriteI2C(Des_addr,0x66,0x06)
    board.WriteI2C(Des_addr,0x67,0x2F) #Most 8 bit of Total Vertical frame size
    
    board.WriteI2C(Des_addr,0x66,0x07)
    board.WriteI2C(Des_addr,0x67,0x80) #least 8 bit of active Horizontal frame size
    board.WriteI2C(Des_addr,0x66,0x08)
    board.WriteI2C(Des_addr,0x67,0x07) #Least 4 bit AV + Most 4 bit AH
    board.WriteI2C(Des_addr,0x66,0x09)
    board.WriteI2C(Des_addr,0x67,0x2D) #Most 8 bit of active Vertical frame size
    
    board.WriteI2C(Des_addr,0x66,0x0A)
    board.WriteI2C(Des_addr,0x67,0x18) #Horizontal Sync Width
    board.WriteI2C(Des_addr,0x66,0x0B)
    board.WriteI2C(Des_addr,0x67,0x03) #Vertical Sync Width
    board.WriteI2C(Des_addr,0x66,0x0C)
    board.WriteI2C(Des_addr,0x67,0x20) #Horizontal back porch
    board.WriteI2C(Des_addr,0x66,0x0D)
    board.WriteI2C(Des_addr,0x67,0x15) #Vertical back porch
    
    board.WriteI2C(Des_addr,0x65,0x0C) #using Internal Timing/Ext. CLK
    board.WriteI2C(Des_addr,0x64,0x15) #enable PG/color bars
    
    
    

    Regards,
    Fadi A.