Tool/software:
Hi FPD-Link team,
I’m running FDP-Link III cameras with the Fusion 2 board on AM62A. Below is my setup:


So far, I've been successfully running IMX390 (based on FPD-Link III) with the above setup. However, I'm running into some issues with OV2312 (also FPD-Link III) which has 2 virtual channels, one for RGB and one for IR. The behaviors I’ve seen are:
When camera connected to CAM1:
- Streaming IR-only: I got flickering images,
- Streaming RGB-only: I didn’t get any image
When camera connected to CAM2:
- IR-only: image is okay
- RGB-only: image is dark
- Streaming IR+RGB: sometimes RGB is bright but flickering, sometime RGB is dark
This same OV2312 camera worked fine with Fusion 1 (FPD-Link III).
I'm using the UB960 driver in the Processor SDK Linux: https://git.ti.com/cgit/ti-linux-kernel/ti-linux-kernel/tree/drivers/media/i2c/ds90ub960.c?h=ti-linux-6.6.y.
Did I miss anything that made the 2-virtual-channel camera not to work?
Thank you.
Best regards,
Jianzhong