Part Number: DP83869HM
Other Parts Discussed in Thread: AM2634, DP83869
Tool/software:
I used AM2634 to connect DP83869 through RGMII and set it to RGMII to 1000BASE-X by starting resistor, LOG shows EnetPhy_findCommonNwayCaps: PHY 3: no common caps found. But RGMII to copper cable can work normally, log as below:
Image loading done, switching to application ...
==========================
CPSW LWIP TCP ECHO SERVER
==========================
EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:0 From 4 To 2
Open MAC port 1
EnetPhy_bindDriver: PHY 3: OUI:080028 Model:0f Ver:01 <-> 'dp83869' : OK
PHY 3 is alive
Starting lwIP, local interface IP is dhcp-enabled
[LWIPIF_LWIP] NETIF INIT SUCCESS
Host MAC address-0 : 70:ff:76:1d:ec:f2 Host MAC address-0 : 70:ff:76:1d:ec:e3 [0]Enet IF UP Event. Local interface IP:0.0.0.0
[LWIPIF_LWIP] Enet has been started successfully
[0]Enet IF UP Event. Local interface IP:192.168.1.250
[0]Waiting for network UP ...
PHY 3: *1 = 0x614d
PHY 3: *1df = 0x41
PHY 3: *c00 = 0x140
PHY 3: *c01 = 0x614d
PHY 3: *c10 = 0x3148
PHY 3: *c19 = 0x10
PHY 3: *c1a = 0x0
PHY 3: *c2a = 0x812
PHY 3: *c30 = 0x3056
PHY 3: *6e = 0x23e
EnetPhy_findCommonNwayCaps: PHY 3: no common caps found
EnetPhy_findCommonNwayCaps: PHY 3: no common caps found
EnetPhy_findCommonNwayCaps: PHY 3: no common caps found
EnetPhy_findCommonNwayCaps: PHY 3: no common caps found
EnetPhy_findCommonNwayCaps: PHY 3: no common caps found
EnetPhy_findCommonNwayCaps: PHY 3: no common caps found
EnetPhy_findCommonNwayCaps: PHY 3: no common caps found
EnetPhy_findCommonNwayCaps: PHY 3: no common caps found