Other Parts Discussed in Thread: LMK05318B, AM625,
Tool/software:
Hello ePHY team,

I am figuring out the connections for the AM625, DP83869HM, and LMK05318B. Other on-going thread: LMK05318: Sync E Hardware connections understanding and Reference.
For a 1000 Mbps Ethernet use case, it is clear that the clock rate must be 125 MHz between the AM62 and the DP83869HM.
However, for the recovered SyncE clock between DP83869HM and LMK05318B, does it matter if either 25 MHz or 125 MHz is picked for CLK_OUT when using 1000 Mbps? Since the recovered SyncE clock provides the frequency accuracy, I don't see why it would matter what frequency is fed into the network synchronizer (LMK05318B).

Thank you,
Jennifer
Applications Engineer
Clocks and Timing Solutions